A simple feature request for bqStudio:
Since the charge and discharge cycles are very long at my current project the Data Graph shows not much history because the greatest Log Interval is 5 seconds and i guess after a fixed number of datasets are on the graph the oldest get removed.
Log Intervals of 10, 30 or 60 seconds would be very useful for me, thus more history is shown in the graph.
Optionally the time after which data points are removed could be made configurable so that more history is visible too.
Would be nice to see this in the next bqStudio release.
Regards
Sebastian