Dear Sir,
Greeting for the day!!!
I am going to design the dual output DC-DC Forward converter as below mentioned spec.
Input : 18-36Vdc
Output: 15V/2A & -15V/2A
Switching Freq. : 250kHz ( Fixed)
All Regulations: < 50mV
Effi>80%
I want to simulate to my design prior to fabricate the PCB and other relevant activity. Sir my design scheme is first converted input voltage 18-36Vdc into 8V at forward topology transformer secondary side due to control the duty cycle going to beyond 50% at 18V input, then 8V is boosted to 15V/2A by Switching boost regulator. I create the two secondary winding for dual outputs ,output-1 is control by the feedback close loop control by the duty cycle through opto coupler. output -2 is unregulated .sir in the balance load condition both output are ok but if my output-1 at no load and output-2 is full load condition the voltage drop at output-2, means cross regulation problem has been occured and pre loading is required to the output-1 for normal operation hence effi. of converter decrease.
Sir i also seen the Synchronous switch post regulator (SSPR) to control the regulation of unregulated auxiliary output in multioutput power supply. how to use SSPR kindly send the application note ,
I am using non TI PWM controller and simulation software, Kindly suggest the relevant application note and schematic.
Many Many Thank You
Regards
Atul Mishra
DC-DC Forward Converter scheme.pdf
Isolated Forward topology.