This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Part suggestion

Hello team , one of my customer VVDN is looking for a battery charging solution

 

Requirements:

1.System Load is upto 2A.(Basically need Power path solution , where the changer ic can support upto 2A drawn by the system )

2.Battery pack is single cell Li-ion battery 460mAh.

3.Maximum charging current is 0.5C and standard charging current is 0.2C.

4. DPPM battery charge

5.Input to the battery charger IC  shall be connected to a Lead acid battery with nominal voltage upto 15V

Please help choose an ic with least part count 

Thank you