I have two TPS65400 devices on my board. #1 has three outputs, SW1, SW2, and SW3 & SW4 are configured in current sharing mode; #2 has two outputs, SW1 and SW2. I need to set ENABLE_PIN_CONFIG=single ENABLE on both devices. This can be done if the version is B or B3; but can NOT be done on #2 if the version is B4. Why is that?
Thanks
Nikko