Hi Team,
My customer confirmed Q1 FET(connected between IN and OUT) is still off even if Vin exceeds UVLO threshold under the condition of EN1=high, EN2=low as the following graph.
There is no battery connection at BAT pin in this evaluation.
Is it a correct feature of bq24230?
I couldn't find a description that correspond to the feature in datasheet.
If he set EN1=low and EN2=high, Q1 FET turns on when Vin exceeds UVLO threshold as datasheet shows.
Best Regards,
Yaita / Japan disty