I installed bqStudio version 1.3.47, connected the PC via the EV2400 to our custom board and started bqStudio. Auto-Detection works and the BQ27742G1 was discovered. The dashboard of bqStudio was able to read the battery voltage and other parameters, all values are updated automatically in the dashboard without any problem.
I created a new project and wanted to use the Parameter Q&A. Here I get the following error message:
Load or Store Action can't find the parameter: Gas Gauging.IT Cfg.Reserve Energy
I looked into the data memory and I could not find Gas Gauging -> IT Cfg -> Reserve Energy. Therefore the error message is right, but I cannot go any further. Parameter Q&A does not work. What shall I do?
BTW 1: I tried the same with the official version of bqStudio, but no luck.
BTW 2: The project typed (basic, advanced) has no influence