This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tiva Connected Launchpad + Fuel Tank MK II Battery Booster Pack Remaining Capacity = 0.0 mAH

Hi,

    I modified the Tiva Connected Launchpad + Fuel Tank Booster Pack (obsolete) example program to work for Fuel Tank MK II Battery Booster Pack. I change the the I2C commands from BQ27510G3 to BQ27441G1 using datasheet as reference. I am getting this reading Remaining Capacity =   0.0 mAH. See, below. Is this normal?

Battpack> status
Battery Capacity: 1340.0 mAH
Remaining Capacity: 0.0 mAH
Battery Voltage: 0.295 mV
Internal Temperature: 32.550 C
State of Charge: 0.0 %
State of Health: 159.0 %
Average Current: -89.0 mA
Recharge Cycles: 0 cyc
Time Until Empty: -3 min

The battery is discharging!

Battpack>

- kel