its input is 10V to 30 V,and its output should be 18V.But now,its out put is changeable from above until 10V.I try to adjust the load terminal ,the value of resistor.Sometimes it changes quickly and sometimes slowly.Now I doubt the C(out) is too large or the frequency(decided by the Rt and Ct from TL494) is too little.Who can tell me the value of C(out) and the frequency have any specific effcts on the circuit.
Thanks.