I work in ARTS Energy and I make tests on BQ34Z100-G1 with BQ34Z100-G1EVM on NiMH battery
We make test of 2C-discharge and there was a capacity fall. When the BQ34Z100-G1 believe the battery was empty, the capacity increases. When OCVTAKEN flag is set, the capacity fall again. It is a problem for us because we want have a good value of capacity and this value has big impact on other value.
After we make a C/3 charge and C/3 discharge to learn capacity to BQ34Z100-G1. During the charge there is nothing the capacity don't change. At the end of discharge it changes his capacity and it was better. When the OCVTAKEN is set the capacity fall again
Can you help us to resolve this problem because we can't understand this variation ?
We have an other problem, the FC flag is set in late. NiMH Delta Temp equals to 0,8°C and NiMH Delta Temp Time equals to 240 secondes. When the FC flag is set, (ΔT/Δt) is bigger than 1°C in 4 minutes, we make our calculation with data give by the BQ34Z100-G1 in log.
We have a third problem, when we make a C/20-charge the BQ34Z100-G1 can't detect the end of charge. When the battery is in overloading his True RC increase while there is not more energy in battery, so there is a important shift at the discharge, there is the same problem with topping charge or a trickle charge
you find 4 log where there is the problem and the gg file in attachment