Hi Team,
The bias current on the high-side MOSFET gate drive is 100uA (max). My customer's comment is that this is a little steep and ideally they would like to get 0A here. They're using external VCC bias and would like to know if it is okay to remove the bias from one of the channels. Is this okay or would it affect the other channel?
I did see the notes in the datasheet regarding "If VCC1 is in an under voltage condition, channel 2 is disabled." Also, "if either VCC is in UV, both channels are disabled." However, I'm not sure if this applies only when using the internal VCC bias or also when using an external VCC bias?
Also, can you please provide some information as to why the high-side MOSFET gate drive bias current is 100uA (max)? What's driving this value in our controller?
Thanks in advance for your feedback.
Best Regards,
Brian Gosselin
AFA Boston, MA