Hi
I am designing the 4 series battery pack. i want to how much parallel cells can i connect or how much Ah battery pack can i balance,protect with bq7692006PW without using external balancing. below is some information for my design
charging current 5-10A
discharging current (nominal) 5-15A, peak 5-25A
Based on the design i have couple of question , please help me in making better pack with TI solution
1. how I select R sense
2. can I use only bq7692006PW with any I2C compatible micro controller like atmega32 or I have to use msp430 only .
3.can I use EVM schematic for my reference design.(page36)
4. what does red cross mean in AFE EVM schematic.(page36)
5. what is the use of D1,D6,C17,C18,C11,C12 AFE EVM schematic(page36)
6. what does NT1, E1,E2,E4,E3 in the AFE EVM schematic.(page36)
7. why D8,D9,R24,R26,R25,R27 used in AFE EVM schematic.(page36)
Thanks
vijay singh