Hi,
i will use the TPS65217 without DCDCx. i know since there are power sequence in logic it is not work without VDCDCx(feedback).
please let me know how do i working if i don't use DCDC function.
thanks,
Chase.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
i will use the TPS65217 without DCDCx. i know since there are power sequence in logic it is not work without VDCDCx(feedback).
please let me know how do i working if i don't use DCDC function.
thanks,
Chase.
Hi Richard.
thanks for your feedback. it was clear.
I have a one more question for TPS65217x
I've been making a circuit for battery charger. I wondering how can I check the work on battery charging? I can’t check battery charging is working good or not. I think it have to need some indicator but I can’t find it.
Chase.
Hi Chase,
In software you can check the status of the charger in the CHGCONFIG0 register.
In the lab, measuring the voltage on the BAT pin should tell if the charger is working or not.
Additionally, you can monitor the charging current by selecting VICHARGE in the MUXCTRL register and measuring the proportional voltage on MUX_OUT. With this, you can actively monitor the charging current if MUX_OUT is connected to a spare ADC in your system.