This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43060 - BOOT pin shorted to ground

Other Parts Discussed in Thread: TPS43060

Hello

We are facing a problem that boot pin of TPS43060 shorted to ground when plugged in DC voltage (35V) into system directly without any soft-start and enable pin was low level (Vout = 0V). In this design we set the output voltage is 51V, but even it wasn't work to continues output voltage, it will be damaged by input voltage pluuged.

Did you ever seen the problem before? Do you have any idea about that?

Thanks,

John