Other Parts Discussed in Thread: BQ24650
Hi,
I am designing a board using the BQ24650 on its lead acid battery configuration, our PCB is working fine. the charger is working properly after find out we misplaced the boostrap capacitor. Now we are testing the reverse polarity protection but we are afraid the PMOSFET we use for it can get damaged. During our tests the MCU we have on the PCB got damaged when the battery was connected backwards. I think it was due to the fact the charger is constantly setting a voltage to check battery connection, so the PMOSFET is actually ON since the voltage at the source is 14.3V (due to the charger) and the gate voltage around 2.8V (1/6 of the source). when the battery is connected backwards I think since the mosfet is ON it damaged the MCU.
We also try the solution using a PTC fuse and a diode, this one works fine but it has its problems (loose battery power when battery is backwards).
We would like a solution with the less power loss possible, we are wondering if you know any other solution we can try.
Here two schematics showing the solutions we have tested,
scheamtics (PMOSFET and PTC fuse with diode).pdf
Regards
Mark