We observe some unexpected behavior related to the BPEXT input.
1. An external 5V is connected to the BPEXT pin, and a 12V input supplied to converter. device is enabled with CNTL pin, everything is fine. If device is disabled by de-asserting CNTL pin, about 500 mV is observed on the output. 12V Vin and 5V BPEXT still applied. If this is repeated with no external 5V on BPEXT and BPEXT grounde dor floating, output drops to 0V as expected.
2. If operating the converter with BPEXT grounded (or floating), an overcurrent alarm is noted. This did not occur with BPEXT tied to 5V. Overcurrent warning set to 20A OC fault set to 26A. Fault is not being tripped. Max load current for rail is about 8A but typically 3A. Another odd thing is when doing a current read back, current reads expected 3A when external 5V connected to BPEXT, but value reads closer to 9A when BPEXT is grounded.