This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3896A - Enable Pin - Vih/Vil

Guru**** 1225732 points

Hello,

For the TPS3896A device,  is there any flexibility on the enable hi/low ( min/max, vih=1.4V and vil=0.4V)?

Looking to run vih=1.350V min and vil= 0.450V max at Vcc = 3.3V.

Are these hard limits or is there more margin? 

Thank you and Best Regards,

Nic