Dear team,
a customer of mine has the following problem with the BQ40Z60.
Battery of 4 series accumulators LiFePO4 MHR32113 from A123.
Nominal capacity is 4500 mAh. Full-charged battery voltage is 14,6V. The Charge Current is up to 2А. The Discharge Current is about 80mА. Minimum voltage of a single accumulator is 1,6V. Maximum Temperature is +65 С.
Problem is in a not-correct determination of charge percentage. Voltage of each accumulator is 3339, 3292, 3613, 3354mV, that doesn't correspond to the Charge. Nominal Capacity is 4300-4500mAh. However, there's in the bqStudio shown 1715mAh, and it's considered as a maximum Charge. Probably, it is because of incorrect coefficients applied, determined by the Chemistry Type...
Question: How could I state them in a correct way? In the Table of Accumulators, suggested in the bqStudio, such accumulators are not available.
Could you please advice?
Thanks a lot in advance for your help.
Best regards,
Massimiliano De Cristofaro
Application Support Engineer - Power Management
ASKTEXAS DiamondLane – EMEA Distribution Support
Texas Instruments Deutschland