Does anyone have an example of the PMBus command sequence needed to change VCCO_VADJ on the Xilinx AC701 evaluation board from 2.5V to 3.3V? I am using the ARTIX FPGA PMBus interface to the UCD90120 controller to make the changes and am coding in VHDL, will not be able to do this using TI FUSION SW.
I need to change the monitor voltage on pin 1, and the GPIO signals 17 and 18. Its not clear if I need to change GPIO15 (VADJ_TRIM).
Thanks for any help,
Rob Curtis