Hola,
I want to use BQ24092 to set the charging current as 50mA with Riset.
According to the equation in datasheet, K/R = Iout, if the output current to be set as 50mA, then:
1. Iout = 527 / 10.8 kohm = about 48mA, is it right?
2. Does the lowest Trickle current only 10mA?below table shows that the Iout(range) is 10mA ~ 1000mA...