This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to analyse the log data in bqeasy

Hi, Ti team

When i do the bqeasy test, i dont know whether the testing process is correctly carried out.

Is there any guide for analysing the log data ?

Another, to the Qmax.  How to check the value compared with real capacity?

                To the Ra_table, again, how to check the ra_table compared with dedicated chemistry ID? Is there any formula?

Best regards

J.C Chen

  • I normally check the accuracy by running a full discharge and checking whether the SOC reaches 0% at the termination voltage. If it is within 1 to 2%, then it is considered to be acceptable. There is not a formula to check the Ra table. The values are typically uniformed through the table and can increase near the bottom.