Hi.
I want to incorporate a load switch that removes power from downstream circuits when they're not required and when the microprocessor goes to sleep. When the microprocessor goes to sleep all its GPIO outputs go into a high-Z state.
Would the N-channel MOSFET of the TPS22959 be high-Z if 3.3V were applied to VIN, a very light load (~300k) was on VOUT and power were removed from VBIAS? Would removing VBIAS have the same effect as applying a low to ON (with VBIAS at 3.3V)?
Does VBIAS need to be high and ON low to ensure N-channel MOSFET remains high-Z?
Can VBIAS and ON be driven from the same microprocessor pin and reliably control VOUT?
Cheers,
Franc