This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206, JEDEC requirement specification for DDR4 VTTREF

Other Parts Discussed in Thread: TPS51206

Hi, 

My Customer has question of TPS51206 about JEDEC requirement specification for DDR4 VTTREF.

*JEDEC requirement

VTTREF accuracy = 0.6V ±1%

There is mentioning of Vref tolerance in data seat P7. 

VTTREFTOL : IVTTREF < 10mA,  1.2V < VDDQ < 1.5V, 48.75%(min)~51.25%(max)

So, I wish not to be satisfied JEDEC requirement.

Is TPS51206 satisfied of JEDEC  requirement of DDR4?