This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting BQ51051B with a ADP5092

Other Parts Discussed in Thread: BQ51051B

Hello-We need to integrate Wireless Power Receiver (BQ51051B) in our design for wireless sensor that uses ADP5092 to charge a 3.7v Li-Po battery from solar cells. The battery is connected directly to the BAT pin on ADP5092. I was wondering if we can also connect the BQ51051B BAT pin directly with the BAT pin on ADP5092? In this case the Battery will either be charged by ADP5092 or BQ51051B. Do I need to add Schottky diodes to prevent reverse current? Thanks in advance!