Hello,
I would like to use a spread spectrum clock.
Does the TPS54020 accept it? Which constraints do I have to consider?
The data sheet (8.4.6) contains a duty cycle range 20%-80%, and frequency range 200kHz to 1200kHz. Is anything else required?
Regards - Frank