Hi All
I'm seeing funny things in the field and trying to understand what is going on.
1) I have a 2 cell in series battery LiOn when I charge the battery to 95% stop and wait then after a while when I cycle the power on the battery and then the gauge indicate 83 % it then stays there for about 4 days before it drops to 82.
2) I charge a 14.8 Volt 4.3Ah LiOn to 100% then leave for a while when I cycle the power on the bettery it drops to 92 % and stay there.
3) 80%of the battery packs does not do this, just here and there I have this issue.
I have a protection board on the battery and a NTC.
Inputs please?
Kind regards
Ben