I read the datashet of LP5907 but I don't find how to set Vout. I need to go from Vin : = 5V to Vout = 3.3V . How do I set this ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
" ... How do I set this ? ... "
You do not 'set' the LP5907 output voltage.
You pick the package you want, then order the preset output voltage you need.
Example 1 : SOT-23 / DBV package, with 3.30V output ...
Example 2 : X2SON / DQN package, with 3.30V output ...
Example 3 : DSBGA / YKE package, with 3.30V output ...