Hi,
I am using the TPS40200 in a flyback configuration and observe the COMP pin railing to 0 for a while before restarting under certain conditions. The COMP pin sticks at zero even though the FB is falling.
ISNS is disabled by shorting pins 7 and 8. And I don't observe VDD falling below 4.1V for a UVLO condition. The soft start pin is connected to ground thru a 1uF X7R ceramic cap in parallel with a 50k resistor, and voltage there looks stable at 3V.
The RC oscillator does not stop during the failure condition. The COMP pin is monitored thru a 100k resistor and the railing to 0 is observed.
What will cause the COMP pin to jump to zero volts? Could the internal 700mV reference be failing? Or could I be missing the soft start observation?
I am assuming that the functional diagram (Fig 4) in the datasheet is close to what is there. Is there another condition that may cause the COMP pin to rail to zero with a falling FB voltage?