This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206 DDR termination regulator S3 and S5 pin connections and current rating

Other Parts Discussed in Thread: TPS51206

I am using TPS51206 in my design for DDR termination voltage. I need VTT to be supplied continuously. From the spec, I understood that S3 and S5 should be high for this condition. In this case to which voltage level should I pull these up? and through which resistor? I think these should be pulled to VDD using 4.7K resistor. Am I correct!? And what is current requirement of S3 and S5 pins!?