This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23751 based POE, disabled from Adapter OR CPU

Other Parts Discussed in Thread: TPS23751

Hi, 

I'm designing an IEEE802.3at type-2 powered device (PD) based on the TPS23751. It will operate with 'Option 3' (power applied to the output side of the converter) for diode ORing external power into the PD. The Adapter will have the priority. In my specific case I would like to disable the PSE source using the DEN pin when the Adapter is present or when a control signal coming from a CPU is asserted, see the schematic attached. Would this work?

Thanks.

TPS23751 POE.pdf