This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS 40170 parallel operation for increased current output

Other Parts Discussed in Thread: TPS40170, UCC39002, TPS40050

Good morning, 

I have a guestion regarding parallel operation of the TPS 40170 buck converter.

My design requirements are the following:

- Input voltage Vin is within 30-48 VDC (Li-Ion, LiFePo battery pack)

- Output voltage is regulated to a stable 24VDC

- Discharge current is regulated  well according to battery max. discharge current (may be 40-60A) 

Since there are no off the shelf solutions for such high current, would it be possible to connect 2 TPS40170 (both rated 25A) to increase Iout? 

Thank you,

Tom