Dear Support team
My customer use TPS61029.And on some board,there is the trace that the electric double-layer capacitor expanded by heat.
We investigates a cause. Customer suppose that Nch FET may be turned on high duty cycle.
Please teach about below question and give advice.
Q1)How much is max duty of TPS61029?
Q2)Is it possible that TPS61029 operate in max duty cycle on the following condition?
◆Condition
Vin:2.6~4.8V
Vout:5V
Iout 580mA max
notice: Load is Electric double-layer capacitor(470mF)
Regards
Tomohiro Nagasawa