I have been designing a device to switch the battery in a vehicle using MOSFETs. The main requirement is the high current conditions during starting (up to 500A). The current design that I have uses the LM5060 to control 4 large high side n-channel mosfets in parallel. This is working pretty well and able to handle the load for most cases.
However the area that I am struggling to get the desired performance is in over current or short circuit protection. I see on some of the other posts that the LM5060 isn't really designed to cope with short circuit conditions. The current circuit seems to fail to switch the mosfets off and puts them into a half turned on state where they subsequently fail due to power dissipation.
Is there another device that is likely to be more suited to this application? I have listed below the desired power specifications of the device.
Current - up to 500A
Voltage - 12 to 24V battery (8-30V maximum)
Size - as small as possible so external sense resistors won't really work for the required current (this is why I like the LM5060)
I would apprieciate any feedback or suggestions that could work for this design. It may be that I have some kind of additional circuitry to shutdown in the event of a short circuit.
Thanks.