Hi TI
According to datasheet.
Sorry, I could not paste the sections described below.
Section 8.2.1.2.9
Page 24
and
Figure 33.
Page 25
If Ro is added will it then limit Vgs at Q1 - or do we risk to damage Q1 with too high vgs?
In the application there is a big capacitance around 1 mF. which is around 1.2J in 0.6 seconds in the constant current generator.
I we add Ro which is bigger then (20V-0,6V)/80mA ~ 240Ohm (0,6V is zenerdiode) it will cause the voltage across gate/source to raise above 20V and the transistor be damaged.
ln section
8.2.3.2.1
Page 28
Here it's mentioned that Ro should be minimum (48V-(4mA*1,5kOhm))/4mA = 10,5KOhm which seems confusing according to limit the vgs.
I hope it makes sense what my concern is.
Last but least, it's also mentioned in the datasheet that a capasitor can be placed from gate to gnd to slow down Turn On. (named C3)
Figure 26 at page 18.
To avoid the high voltage rating of the capacitor.
Can it then be connected between gate and source on Q1. Then it should only be rated 20V?
Thanks in advance.
JW