This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Low current boost converter

Other Parts Discussed in Thread: LM5022

Hi I am working on a high current boost converter  delivering max 200V 2 mA from 14-20VDC

And with low Rushing and peak currest when enabling the device (<50mA) becaus I can only have an 80mA Fast fuse at the input.

I have a circuit with LM5022 which is workin a bit  after playing with components but the caculations around it does not mach my values.

and the power consumptio of the circuit is higher tha I would expect. At 1mA output current I have about 40 mA input current.

I know the device uses<4mA so lots of energy gets lost.

I have some trouble defining the L and Current sense resistor. I expect I would calulate this current sense resitor for about 20 times Iout so 40 mA

Am I correct this would mean 0.5V/0.04=12.5 ohm?

What value for the L would I need if this is correct?