This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Help on selection of DC-DCs for ganged biasing of Op-Amps

My requirement goes as belows for biasing a set of 30 opamps at a time

Input available from battery : 28V

1. +2.5V @ 1A(o/p voltage @ o/p current)

2. -2.5V @ 1A

3. +5V @ 1A

4. -5V @ 500mA

first of all is it better directly connecting all dc-dcs to one battery voltage input or use a LDO in between to bring the voltages down to +5V

and then use dc-dcs to attain maximum efficiency, kindly suggest a high efficiency approach ?

28V to 5V LDO followed by individual dc-dcs ?

for now i picked

LMZ4201 for both 1 & 3, the dc-dc may provide 80% efficiency with 28V input to 5V and 2.5V conversion

how about bringing 28V battery input to down to 5V and then using same dc-dc to distribute +2.5 +5V or anyother based on requirement,?

Kindly provide help on generating 2 & 4