Hello team ,
My vustomer VVDN is looking for a solution in DC/DC converter with the specs below
1) Vin=5V max Vout= -15V Iou=0.7A max
2) Vin=15V, Vout=1V to 10V , Iout = 0.5A max, Output voltage should be configurable through SMBUS or PMBUS or I2C or SPI interface in run time.
Converter , controller or module is acceptable
Please let me know the right part to suggest for the above parameters
Thank you