Hi team,
My customer is using the BQ24295 now. And meet some problems.( The battery is 3.7V/1920mAH)
1. When the battery is fully charged, the INT pulse only happen once, but from the datasheet, the INT pulse should be continuous.( we read the REG09, it's 0x00)
2. When we remove the battery when charge or finish charging, the INT will trigger every 256us, the REG09 is 0x00 too. Why? From the datasheet, the INT trigger shouldn't be continuous.
3. We also test the State pin, but the frequency is 20hz not the 1Hz.
BR
Frank