Dear Sir,
I have power supply design that have been using UCC28740 and the design is base on one of TI reference design.
Could you help me review schematic, layout of it and give me some comments to pass UL certification ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I have power supply design that have been using UCC28740 and the design is base on one of TI reference design.
Could you help me review schematic, layout of it and give me some comments to pass UL certification ?
Hello Nguyen,
This is not a service generally provided by TI. However, I will try to make some recommendations.
To meet UL the design needs to meet creep edge and clearance specifications.
1. Primary to secondary 8 mm, 4 mm air gap.
2. Isolation transformers must be design for reinforced isolation 4.5 kVA
3. You can use component (FET, Diode) ratings and lead spacing's as guide to how far apart the traces should be.
4. The PCB needs to be made of material that meets UL94V-0
Please note to other e2e members if I had missed something or you have something further to add please feel free to respond.
Regards,
Mike