This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPC Tool Generalization for Multiple Cells

Good morning,


I have a question regarding the GPC tool. Given the scenario that I have a large quantity of 18650 cells(all of which are the same model), would a golden GG file need to be generated for every single cell in regards to product deployment? I do realize that the learning cycle will improve the estimation accuracy of the IT algorithm. It is my understanding that the benefit of the golden GG file is for thermal optimization, and I know that not all cells will be manufactured equally, but I see this as minimal if the learning cycle is sufficient. This is why I wanted to consult an experts opinion.

Thanks

Blake