I plan to use multiple Li-ion cells (18650, mostly I need 4 cells) in parallel connections for portable devices, and about to realize the following functions:
2A/4A Charging (with protections), precise percentage (1% or so) of the total electrical volume, I have chosen BQ29700(Protection),BQ24195(Charge IC), BQ27542-g1
So I have some questions:
1.Can I use one gas gauge for multiple cells in parallel connection? What should I concern, other than single cell uses?
2.Some of the 18650 cells already have protection board built in, (usually DW01+ 8205A, which is more expensive than cells only), do you suggest I use the built in ones or BQ29700? Or, do you suggest I use both if I need protections of each cells?