This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40z50-R1 Calibrate with 50% current

We have calibrated our packs so that under any given load, the BQ shows 50% of the actual current. This is because our application can pull more than 32A and we had to scale the current readings. Everything else is obviously adjusted accordingly.

I looked at the pdf on 'High Capacity Packs' and noticed that this effect was achieved using a 4A load while telling the BQ it's only 2A. For our learning cycle, we used a 2A load and told the BQ it was 1A. Would there be any difference between the 2 methods (especially in the accuracy)?

Thanks