This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51220A / VREG3,VREG5,VREF2

Other Parts Discussed in Thread: TPS51220A

Hi

i use TPS51220A for power , vout to 3.3V and 5V

vin is about 12V

i have some trouble

1. when vin is supplied, VREG3 is on, but voltage is 3.7V~3.8V , it seems to over spec 3.3V

2. when EN is to 3.3V, no power on VREG5 and VREF2, 

for above two points, it seems TPS51220A not working normally

could you help to give me some suggestion 

thanks