Dear TI,
I've recently Sealed a fresh BQ34Z950 IC but I didn't note down the UnSealKey from the device to Unseal it.
Is there any way that I can Unseal this IC? Or is there any default UnSealKey for a fresh IC?
Thanks in advanced.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The default unseal codes are 0414 3672 and the default full access codes are ffff ffff. The codes will not work if the user has changed them.
Thomas,
Thanks for the given answer above. Now I've Unsealed the fresh IC from Sealed mode.
I've another question:
Using the same IC, after I disconnect the Pack+ pin which was at 16V and reconnect it back (same at 16V), the IC is back to Seal mode. The [FAS] and [SS] flag are turned to red (set).
At this stage, I just want to power up the IC thus no battery or battery simulator connected to the IC.
Is it normal that the IC behaviors like this with the condition above?
The device will reseal automatically, if it gets reset. Removing reapplying the voltage would cause a power-up reset.