My customer is using the TPS61195 in a backlighting application. They are trying to determine a system fault signal to indicate a bad backlight and had the following questions:
1. BL_STAT: What is this bit mean? If the BL_STAT = 0 does it indicate a bad Backlight driver? If the BL_STAT = 1 indicates a good Backlight driver (NO Faults)?
2. 2_CH_EN and 1_CH_EN : What this bits mean? Are this the LED strings fault? Which faults (ex. Open, shorts, etc.)? What happens to BL_STAT and FAULT bits when the CH_EN reports a fault?
3. FAULT: What is this bit mean? If the FAULT = 1 does it indicate a bad Backlight driver? If the FAULT = 0 indicates a good Backlight driver (NO Faults)?
The datasheet is a little light on details for these. It is not clear if BL_Stat changes on fault conditions. Also, the Fault indicator seems to indicate "any fault except LED open and short occurs"... so this only toggles on thermal shutdown and overcurrent? Is a short condition the same as overcurrent?
Thanks,
Dan