This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Doubt regarding core loss calculation for forward converter

Hi friends,

I have designed a forward converter transformer using flux density 0.2T. I have used 0.2T for my minimum number of primary turns calculation. But when i referred some documents they are taking half of flux density(0.1T in my case) to calculate the core loss. (using equation PL = a*f^cB^d  where P is in mW/cm3,B is in kG and f is in kHz).
what is the flux density i need to take for core loss calculation?. If the document is correct what is the reason for it? Please help me for this.

Regards

Aneesh

  • Hello Aneesh,

    The core-loss equations and core-loss curves of the ferrite material datasheets use peak flux density, which is the zero-to-peak value, not the peak-to-peak value.  This is a consequence of traditionally using sinusoidal excitation for core loss measurements.  The ac flux passes from positive peak through zero to negative peak, and back again. For SMPS design, a forward-mode flux traversal usually goes from near zero (maybe some remnant flux) to the peak and back to near zero.  But this flux path can be considered as a peak-to-peak swing centered around a DC offset at 1/2 of the zero-to-peak flux density. 

    Since the losses are based on the ac traversal around the B-H loop, and this loop is centered around the 1/2-point of the peak flux, only 1/2 of the peak flux density is used for the loss equations and curves.  This application note Magnetic Core Characteristics (2) slup124.pdf has some discussion on this topic, on page 2-5, that explains it better than I can.    

    Regards,

    Ulrich

  • Hi Ulrich,

    Thanks for your valuable answer. So as a conclusion i need to take 0.1T for loss calculation if i take 0.2T for my primary Turn calculation for forward converter right?

    Regards
    Aneesh
  • Hi Aneesh, 

    Yes, that is correct.  Use 0.1T for your loss calculation if your delta-B, based on turns, voltage, on-time, and core area, is 0.2T.  

    Regards,

    Ulrich

  • Hi Ulrich,

    Thanks for your explanation. I have one more question regarding the core loss of output inductor. My Output current is rated to 5A. But my peak to peak ripple current in the inductor is 30% output current current ie 1.5A. So while calculating the core loss of my output inductor i need to find the flux density(B) corresponds to 0.75A(half of 1.5A) as per your previous explanation Right?. Correct me if i am wrong. Could you please share me if you have any documents which discuss this topic.

    Regards
    Aneesh
  • Hi Aneesh,

    That is also correct.  The same flux density treatment applies to inductor core loss as in transformer core loss.  However, be aware that the delta-B is the result of a delta-H corresponding to a delta-I through the inductor.  It may be misleading to think of finding the flux density (B) which corresponds to 0.75A.  To be more precise, you are finding the delta-B which corresponds to the delta-I of 1.5A around a dc operating point of 5.0A, and using 1/2 of that delta-B for your core loss calculations.

    I make all these precise distinction because, for a buck-PWM output inductor, the permeability may reduce as dc bias current increases, so the delta-B for delta-1.5A may be different at a 5-A bias than it is at a 2-A bias level, for example.  This is especially true when using powdered-iron type cores.  If you have a gapped-ferrite core for the output inductor, the inductor properties generally stay linear until the core saturates, where the properties will change rather suddenly.  With powdered-iron cores, the core will partially saturate with higher dc bias current and the delta-I will result in a wider delta-B than at low loads.  I suggest to review the design information provided by Magnetics, Inc. and Micrometals concerning their powder-core products for core loss and other considerations. 

    But, assuming you have a gapped-ferrite inductor, its core loss treatment is very similar to that of a ferrite transformer.  More on this can be found in an application paper Indtr & Flyback Xfmr Design (5) slup127.pdf with an example on page 5-9.  This paper and the others I have mentioned previously are all found in TI's Magnetics Design Handbook which can be obtained here: https://www.ti.com/seclit/ml/slup132/slup132.pdf .  I find this handbook to be an invaluable source of guidance on basic and advanced magnetics design issues.

    Regards,
    Ulrich 

  • Hi Ulrich,

    Thanks for your valuable support. I have a problem regarding the temperature rise calculation of my core. Most of the core manufactures are not providing the thermal resistance details of their core. So after getting the core loss also i am not able to calculate its temperature rise. I have seen from some documents E55/28/21 core is having Rt=11 deg/Watt. So my doubt is how i will calculate the temperature rise of the core after getting core loss?. Can you share me some documents which discuss the above topic?

    Regards
    Aneesh
  • Hi Aneesh,

    The issue of temperature rise for a magnetic component does not have a precise answer. There is a general formula that usually makes a good estimation of delta-T that has been quoted in several magnetics vendors' literature. It has yielded reasonable results, in my experience, and I believe that's why everyone keeps using it. The following section has been copied from the Magnetics, Inc. website from one of their help files:

    "The observed temperature rise depends heavily on environmental factors such as ambient temperature, airflow, geometry, and the thermal conductivity of all the materials involved. A useful first cut equation relates the surface area of the magnetic with the total losses to yield an approximate temperature rise (from room temperature, in still air):

    Rise (°C) = [Total Loss (mW) / Surf. Area (cm^2)] ^0.833

    For example, assume a transformer with copper and core adding up to about 0.6 W, and having a surface area (top, sides and bottom of the wound device) around 15 cm^2. Then the approximate ΔT is [600/15]^0.833 = 22°C.
    Other factors that should not be overlooked are skin and proximity effects in the copper conductors, and fringing effects. The fringing problem occurs with gapped cores, where flux at the gap can intersect with copper near the gap and generate eddy currents. It is possible for the losses due to those eddy currents to exceed the total core losses in the inductor."
    (Excerpted from: https://www.mag-inc.com/design/design-guides/designing-with-magnetic-cores-at-high-temperatures )

    It is important to use the correct units of mW and cm^2, and to make sure to include ALL of the losses, core + copper loss, in the total loss factor. Keep in mind that it is an estimation, although usually a good one, applicable to room temperature and still air. Moving air, higher ambient, nearby heat, and/or enclosed spaces will affect this estimate, but it is usually apparent how these different conditions can either decrease or increase the original estimate. Once your paper design is finished to your satisfaction, the prototype transformer or inductor should be constructed with a thermocouple embedded at the hot spot (usually under the inner most winding, or between bobbin and core) and operated at maximum conditions to verify your expectations.

    Regards,
    Ulrich

  • Hi Ulrich,

    I have doubt regarding the transformer turns equation. The transformer equation which is mentioned in magnetic inc document for square wave is E=4B*Ac*N*Fs x 10-8 (square wave). But while designing transformer minimum number of turns every document follows the equation N=(E*D/Ac*B*Fs)

    Where E=Voltage

    B=Flux density

    Ac=Core area

    N=Number of turns

    Fs=Switching frequency


    If we give same values to both equation we will get different number of turns. Why this difference has come?. Which is the right equation?. Can you explain me the reason?

    Regards

    Aneesh
  • Hello Aneesh,

    Both equations are correct, but the difference lies in the units that are applied to the variables.

    The equation from the Magnetics, Inc. handbook is based on the CGS system of units (centimeter, gram, second), which is an older system used in the early days of magnetics design. In the past few decades many documents and companies have moved to the SI system (metric) of units, on which the second equation is based. TI’s application note “Introduction and Basic Magnetics” slup123.pdf discusses this topic.  This app-note is the first paper in the TI Magnetics Design Handbook that I mentioned  in an earlier reply.

    Because of the differences in units, once you start a design in a particular system, you need to continue to use the same system throughout the design to avoid conflicting results. For example, a couple of the major differences between the two equations are core area in cm^2 or m^2, and flux density in Gauss or Teslas.  On the other hand, Volts, turns (N) and seconds are the same in both systems.

     Although it is good practice to choose one system and stick with it, a lot of very useful design guides and informational papers were and are written in either system, so be prepared to have to understand the concepts presented and translate between the two unit systems as necessary to get the most out of the information presented.   The concepts are the same even though many units and equations are different.

    Incidentally, the Magnetics, Inc. equation, which includes a factor of "4", applies only to a square wave and the "B" is 1/2 of the total delta-B as shown in their Figure 1.  This "4" accounts for a factor of 2 to cover 1/2 of the switching period (because of the square wave) and another factor of 2 to cover the full delta-B.  My preference, and that of many other application papers, is to use: delta-B = (V*T*10^-8)/(Ae*N) where V is the dc voltage applied to the inductance, T is the time applied in seconds, Ae (same as Ac) is the effective core area (in cm^2 for this CGS equation) and N is the number of turns of the winding.  Then use 1/2 of this delta-B to determine core loss.   This Volt-second method is not strictly limited to square wave-shapes.  The product L*I can often substitute for V*T (based on V/L = dI/dt) when the inductance and peak-to-peak current are already known and V is a dc quantity.   

    Regards,
    Ulrich

  • Hi Ulrich,

    Thanks for your Explanations. This information really Helped me.


    Regards
    Aneesh
  • Hi Ulrich,

    I have a doubt regarding the pulse transformer design equation mentioned in the below application note.

    www.x-relsemi.com/.../AN-00371-13-XTR40010-Pulse Transformer Design Guidelines_for web site.pdf

    In their application note they are calculating the Ampere Turn first. They got 55.4 A-T. and their drive capability is 16mA. So they are stating that " the number of turns that will make the core enter into saturation is 3437".
    But normally When N increases Flux density will reduce and the chances of getting in to saturation will reduce right?
    And saturation will occur when we are operating with higher flux(ie Lower Number of turns). But they are stating more than 3437 Turns will result in a saturation. Could you please explain this?.

    Regards
    Aneesh
  • Hi Aneesh,

    It is good to read other literature to gain insight into others’ perspectives of magnetics design, and to experience a broader view of the overall range of applications. The design of signal pulse transformers relies on optimizing different aspects of the magnetics than that of switched-mode power conversion, or that of audio amplifier transformers, or of power-line distribution transformers. The basic magnetics theory and equation set hold true for all of them, but each sub-topic will emphasize a different set of parameters to be optimized for the particular application.   

    In the case of this pulse transformer design, the issue of saturation is handled by the author in a different manner than we have been previously discussing. The ampere-turn approach is equally valid for all magnetics, but I believe the X-Rel Semiconductor author chooses to use it because, for his choice of core shape and material, the relative-mu is a known quantity. In power magnetics, the relative-mu is generally unknown, whereas the Volts, seconds and core area are specified.  Given enough theory and math, we’ll find that the two different Bmax equations can be derived from each other, but I’m not going to go into that here.   The only objection I have of the app-note is the author’s use of the word “ratio” when discussing the current*turn product.  A*turns is a product, not a ratio, but the math is not incorrect, only his terminology.

    From the paper on basic magnetics (slup123.pdf) we see that the flux density B in a material is equal to the permeability mu (u) of that material multiplied by the magnetic field strength H applied to that material: B = uH. We know a material such as ferrite has a maximum flux density capability Bmax above which it saturates and cannot increase anymore.  From B = uH, we infer that Bmax = uHmax, assuming that mu (u) remains the same.  We need mu to remain constant (or semi-constant) to keep the inductance equal to a design target.  Actually, when a core saturates and B stops increasing with higher H, it is the relative permeability which collapses to ~1 and so does the inductance which depends on that permeability.  The magnetic field H can increase any amount (depending on how you drive it) but B will not increase above Bmax because mu decreases.

    Anyway, the H field is generated by ampere-turns over an effective magnetic path length (le). For a given core shape, 100 A in 1 turn yields the same H as 1 A through 100 turns.   The X-Rel app-note uses the equation NI=(Bmax*le)/(u) which can be rearranged as Bmax = u(NI/le) which is = uH. 

    Now to finally address the issue of higher turns increasing B vs. higher turns reducing B. Both are correct, depending on what other parameter is being held constant.  For power magnetics, B = Vt/NAe = LIpk/NAe.  In the pulse magnetics app-note, B = uNIpk/le.  We can equate the two and see that LIpk/NAe = uNIpk/le and rearrange to get L = N^2(uAe/le).  The inductance depends on the turns-squared and the Al (A-sub-L) factor, which is a property of a particular core shape and material.  Notice that the L is independent of Ipk as long as the material does not saturate (relative mu goes to 1).   But adding turns will increase L by the square of the turns, so L can go up dramatically, but Ipk will be lower for a given Volt-sec product. In the power magnetics case, we often target a specific L for the transformer, so the relative mu must be changed (generally by gapping the core, or mixing materials as in powdered iron).  In this case the turns N appears in the denominator of the B equation, since reducing the mu keeps the L from increasing and counters the increase in H-field (from N*I).  In the pulse magnetics case, mu is kept fixed, so for a given Ipk, adding turns increases L and increases H, and the N term appears in the numerator.  Therefore, it is important to avoid too many turns or the core will saturate.  It is a bit unfortunate that for the X-Rel application, the number of turns that could saturate the core is about 3400 whereas the number of turns found to be needed for operation is only 12.  Obviously, this difference shows that there is no danger of saturation, but the magnitude of the difference rather diminishes the point of the Bmax calculation, and it seems almost superfluous.

    But it is always important to check the maximum level of B to avoid exceeding Bmax, regardless of which equation is used. The choice of which equation to use depends on which of the system parameters you know, which are targeted values, and which are derived from other constraints.  I urge you to keep reading all kinds of literature on magnetics design from many different sources.  The math and physics are rarely ever wrong because peer-review will drive out the incorrect or mistaken papers, but the various perspectives of the surviving papers can be invaluable to building a broad knowledge base for understanding a wide variety of magnetics design considerations.

    Regards,
    Ulrich

  • Hi Ulrich,

    I have read a document of DCM flyback converter design. In that document they are discussing about stepped gap transformer. The air gap in the core is like a stepped one not the uniform one.Could you please tell me the advantage of stepped gap core transformer?. How it improves Load and line regulation.

    Please refer page number 5 in the below pdf
    www.mouser.com/.../2-8.pdf

    Regards
    Aneesh
  • Hello Aneesh,

    A stepped-gap core allows higher primary inductance when the current is low and low inductance when the current is high.  Use of this technique is not common, but when used, it is usually used for output filter inductors.  Since a flyback transformer is actually a coupled-inductor, this technique can be applied to it. The following file discusses this in more depth. Link:

    I don't have any experience using a stepped-gap or "swinging choke" design for a flyback application, so I can't explain or attest to the claim of improved load and line regulation.  It is interesting to note that, after making a mention of this "advanced technique", the article dismisses it as too advanced for further discussion and proceeds with the usual DCM design. I'm sorry that I can't help you more on this topic, but I recommend searching the internet for other information on stepped-gap cores.

    Regards,
    Ulrich