This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100-g1 Vil level

Other Parts Discussed in Thread: BQ34Z100-G1

Hi There,

I have a system working with multiple bq34z100-g1 SOC IC's.

I need to change the configuration a little bit and am seeking clarifications on the Vil levels.

I am wondering if the datasheet value for Vil-max for SDA and SCL is in fact 0.6V as stated in the datasheet - it doesn't state particular pins unlike the other parameters.

This seems quite low (should be 0.3 x Vdd) for I2C, and would not be compatible with the part i need to use to talk with it (bi-directional isolator)

Can you please confirm if the SDA and SCL Vil-max is in fact 0.6V or 0.3x Vdd?

Is there any way to raise the Vil-max level?

Thanks,

Bryce