Hi, I've finished the fundamental setting of the battery pack(2 x 12V Lead Acid Battery), then I enable the IT(Impedance Track) and start running learning cycle.
For the learning cycle, I pick a new battery pack(which has not been used since being purchased and it's capacity is approx. 80%). I start charging with it until the charge termination is reached, then I rest the battery until the OCVTAKEN flag is set. Then I start discharging it by C/5 until the terminate voltage is reached, then I rest the battery until the OCVTAKEN flag is set. Again, I reloop the procedure of charging and discharging until the OCVTAKEN set.
After 2 times repetition, I found that the "Update Status" of the bq34z100-g1 in "Gas Gauging" setting is still 0x04. From the datasheet, it says 0x04 means "Impedance Track is enabled but Qmax and Ra data are not yet learned". I think it's supposed to be 0x05 after the 1st time charging-discharging and become 0x06 after the 2nd time loop. Does anyone know the reason? Thanks!
(By the way, I've attached the gg.csv file I export after 2 loop of learning cycle)
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/201609191700.gg.csv.7z