Other Parts Discussed in Thread: UCC28070, UCC25600, UCC28950, UCC28061, UCC29950
I have to design and build a AC-DC converter which will have to deliver 25V DC at 120A and the efficiency must be above 90% including the PFC stage, so the DC-DC converter itself must be at least 92.5 to 94% efficient. I was thinking to build the PFC using the UCC28070 and for the DC-DC converter i had to choose between a Phase-Shift FB and a LLC Converter. I want to approach an LLC Full-Bridge converter design and from all the IC's which are available, i would like to use the UCC25600 since it has adjustable DT and no gate drives, which offers me flexibility in driving the power stage. For the rectification i will consider Synchronous rectification. The primary DC voltage i also want to increase at 420-440V DC, to take advantage of the lower switching losses and minimize the conduction losses. I plan to use Infineon Cool MOS transistors.
Now the question is, did someone used this IC or at least the LLC Full-Bridge topology at this power level ? What kind of difficulties i should expect ? Would be practical to use this topology at this power level ? And most important, Reliable ??? I do know that there are some issues regarding MOS-FET's failure rate in LLC converter at low load or no load due to the body diode conduction.
Please advise.
Thank you very much.