This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV704 PSRR

Hi, folks

We are trying to replace NJM78L05UA to TLV70405.

The conditions are below,

VIN=7V, VOUT=5V, IOUT=30mA

For PSRR point of view, the NJM78L05UA better than TLV70405 in DC area (< 100Hz).

Since TLV70405 is low drop regulator, I understand that it is different from 3T.

But I would like to know about the PSRR if the TLV70405 have enough drop voltage? (i.e. 2V)

Can we observe the improvement or not change so much?

Also could you show me the PSRR data for TLV70405 at VIN-VOUT around 2V if you have?