This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5035 or LM5039 / Without Synchronous Rectification

Other Parts Discussed in Thread: LM5035, LM5039

Hello;

I'm working on an isolated DC/DC converter application: 72V to 24V/6A. The topology I chose is half-bridge and I want to use LM5035 or LM5039 because they both have built-in high side gate driver outputs.

App. info suggests to use synchronous rectification switches at the secondary side for better efficiency and performance. Since the output voltage is about 24VDC, I think I don't have to use synchronous rectification.

So the question is, what if I don't use SRx outputs? Because I prefer using diodes instead.

Thanks in advance.

  • Rohat,

    If you do not need to use the SR drive capability (if you have diode rectifiers), then you can just leave the SRx output pins open or floating.

    I hope this helps answer your question, if so please click the "verify answer" button.

    Thanks,
    Bernard